This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc2591 vs cc2595

Other Parts Discussed in Thread: CC2595, CC2592, CC2520, CC2538

Hi,

In some products our company has been using cc2591 together with cc2520 for a while. There is a very good application note regarding this combination:

http://www.ti.com/lit/pdf/swra229

However I've not been able to find the corresponding information for the combination cc2520 + cc2595.

In particular I'm interested in what the TXCTRL and AGCCTRL1 registers shall be configured to. For cc2520 + cc2591these registers should not have the default values, new values are suggested in the application note mentioned above.

In addition to that, the TXPOWER register values are of course different from running the cc2520 as standalone. In the above application note new values for cc2520 + cc2591 are given for the TXPOWER, I'd like to have something similar for cc2520 + cc2595.

I've compared the datasheets for cc2591 and cc2595 and as far as I can see, the gain and maximum output power differs between the two products, so I assume I cannot use the same values when using cc2520 + cc2595 as with cc2520 + cc2595.

Thanks in advance for any information/documentation on this.

Br Håkan