This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

A1101R04 range Issue



Hello,

For one of the project initially I used A1101R08 (868MHz). But the range was less when our customer tested in site. All the modules were mounted inside the plastic enclosure.

Now I have changed the modules to A1101R04 (433Mhz) thinking the penetrating will be better. In both the cases the datarate was 4.8Kbps.

For A1101R04 I am using the below settings from Anaren.

Without the enclosure the range is good but when the modules are placed inside the plastic enclosure the range is less then 20Mts with external antenna.

Can you please let me know the cause and solution for the same.

Thanks in advance.

BR,

Sreekanth