Hi,
I've used SimpliciTI in order to make an RF-communication. The transmitter sends numbers from 0 to 100. Receiver should toggle LED when it receives the number. But the software works properly with some numbers for example 8,9, etc... For the rest leds are not toggling but only the green led is set which notifies that connection is succesful. Transmitter sends a valid message but the receiver can not receive the exact message. What can be done about this situation? How can I ensure that the data is transmitting reliable?