I've been developing custom boards with the designs from DN031. In the design note, I see good numbers for gain and directivity but how do these numbers translate to physical range with line of sight? The reason I am asking this is because I have made custom boards for #6 and #10 from DN024 and observed a huge difference in range:
- Board #6 (90% efficiency): Range of 100m LOS
- Board #10 (60% efficiency): Range of 10m LOS
I understand that efficiency is squared since it affects both the receiver and the sender but a drop from 100m to 10m seems too large.
In addition, I see the note from DN031 mentioning that the antenna needs to be tuned. Am I required to change the values of Z101 - Z104? Or are they fine as is? Currently, I am using the exact components for Z101 - Z104 as stated in DN031. Also, not sure if this matters but instead of doing impedance matching with multiple discrete components, I am using a 915 MHz balun from Johanson.
FYI, we don't have a network analyzer here so I am contemplating getting external help to tune my antenna. Or if it is even possible to tune it to increase its range. Lastly, if anyone has a good contact for antenna tuning in Shenzhen, please send me an IM!