Other Parts Discussed in Thread: CC1200
Is it feasible to use the ASK demodulator on the CC1200 for PPM (pulse position modulation) decoding? Packet decoding on CC1200 not necessary, this can be done by the host MCU, basically the CC1200 would only detect the carrier pulses as ASK and the MCU would measure the interval between each received pulse to correctly decode them as bits.