This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Logic Gate Minimum Input Edge Rate

Hello,

I am looking for some information pertaining to the minimum edge rate for a 54AC00 Nand Gate. There is a recommended minimum of  125mV/ns but there isnt an absolute minimum rating. I am looking for the absolute rating where there could be device damage if the minimum rate is exceeded. Thanks for any help you can provide.

Josh