This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F05 Flash API Code Limit

I recently downloaded the F05 Flash API (v1.00).  It appears that the F05a.a library file was created with a code limited version of IAR's software.  When I try to use that file in my project, I get errors telling me that I have gone over the code limit of 32K.  I have a standard license for the software, so code size should not be an issue.  I contacted IAR, and they said that if any of the library files in the project were created on a code limited compiler, then the whole project becomes code limited.  That applies even if you are using a fully licensed IAR product. Would it be possible to get a non code limited version of the F05 Flash API library file?