This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

V62/03628-02XE



TLV5638MDREP is a dual 12 bit DAC with a -55 to +125C (Mil) temperature range. The part is also orderable as part number V62/03628-02XE which is a DSCC MIL part number. The V62/03628-02XE documentation doesn’t seem to show any additional screening or process improvements. 

What I want to find out is:

  • Do V62/… part numbers have any additional screening or other differences, other than documentation, that differentiate them from the standard TI part number items?
  • How can I get a list of screening and testing performed on either V62/… or standard TI part numbered items?

 The V62/03628-02XE has long lead times and so I want to know the benefits of using these over the TLV5638MDREP. 

Thank you.