Hi all,
Can i use UC1825 PWM controller IC for synchronous rectifier buck converter?
Can i drive its error amplifier output externally to achieve CC mode compensation to CV mode compensation networks?
Best regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
Can i use UC1825 PWM controller IC for synchronous rectifier buck converter?
Can i drive its error amplifier output externally to achieve CC mode compensation to CV mode compensation networks?
Best regards.
Dear Ramesh,
1.Yes and we need rad-hard ICs.
2. 100V input, 50-85V output, at CC mod 5A output current. By adding additional componenets to drive mosfets , we may use TPS50601-SP.
3. For above specifications, target efficiency is %93.
4.Can i use UC1825 for synchronous buck converter application?
5.Yes, so we need CC to CV mod transitions at control loop
6. How can i do that? By connecting inverting and non-inverting pins to ground and drive its output from external compensations signals suitable?
7. At this mode,will i connect internal reference to inverting pin? Therefore, there will be no need to drive internal error amplifier from external E/A. Am I right?
8.Yes, but it is not satisfactory to be able configure external E/A voltage and current compensation loops. There is no space qualified PWM IC that has two error amplifiers in it at TI products- am I right?
Looking forward to see your response.
You can get contact with me by e-mail.