Other Parts Discussed in Thread: UCC2805, UCC1805
Hello, I am using the UCC1805 in an isolated flyback and the error amplifier is not acting like an op-amp. With my compensation the output is 180 degrees out of phase with the current. I am using a type 2 compensation network. I have a UCC2805 and I have hooked its error amp like an inverting op-amp and applied different loads to the feedback and when the load is light it is pretty good but the more I load it the worse it gets. Any suggestions?