This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS4511-SP: THS4511-SP board layout considerations for the ceramic dual flatpack

Part Number: THS4511-SP

Hi all,

1. Is there a gerber file available for the ceramic dual flatpack option available?

If not, what should be considered in layout?

The long leads will add additional inductance compared to the smt version.

/Mark

  • Hi Mark,

    We did not build a marketing EVM when we released the THS4511-SP.  Instead, we point users to the commercial EVM for device evaluation.  Here is the link to the trim and form specification which we have used at Fancort.  Users are welcome to trim and form the device as they see fit as there are tradeoffs to be made with board level reliability (BLR) and the trim and form. 

    www.fancort.com/.../16LEADFP.pdf   

    Regards,

    Christian