Other Parts Discussed in Thread: OMAP3530
Team,
Has the AM3517 undergone any radiation testing? Do we have a radiation testing report available?
Thanks in advance,
Anthony
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We need more information on the request. Is this a question about the SER performance (soft error rate) of this device? or something else?
Hi Wade,
Thanks for the comments.
Looking at the datasheet AM3517 is 65-nm CMOS Technology. I think it should be comparable to what is used for OMAP3530-hirel.
May we be have data available for other processor in the same technology node like OMAP3530-hirel?
http://www.ti.com/product/omap3503-hirel/descriptionDo you think that some of the OMAP3530-hirel data could be useful for AM3517 too?
thanks in advance,
Anthony
Hi Anthony,
Wade is correct, unless the device is marketed for space (-SP) we do not have any space radiation data. getting radiation data is time-consuming and expensive (especially SEE of processors) so we generally focus our efforts on popular space-rated products.
In terms of leveraging off space products that were made in the same process technology, IF the same SRAM bit cell were used in both products you could probably use SEU data from a related -SP product and the answer would not be too far off. For TID this is a much more hit-or-miss proposition since unless both products you are comparing use exactly the same components (BJT, MOSFETs) you might take some encouraging TID data from one product but then be surprised by how bad the TID in the other product is and this would be due to the use of a component that was TID weak limit the performance far below expectations based on the other product which did not contain this product. SEL is very much layout dependent and component dependent so again it is very hard to use data from a different product to guesstimate the SEL performance of another product.
Basically non-space rated products are NOT recommended for space use. Thus, if you must use it (because a suitable -SP grade product does not exist) then I would suggest that you radiation test it for TID and SEE.
Sorry I cannot be of more help,
Rob
Hi Rob,
Thanks a lot for clarifying.
I checked the TI web. None of the Sitara device are marketed for space so far.
The two TI processors that are marketed for space are below:
http://www.ti.com/lsds/ti/space-high-reliability/processor/c6000-dsps-products.page#p1498=Space
I assume that the features listed like:
Single Event Latch-Up Immune to LET = 117 MeV cm2/mg
Radiation Tolerance: 100 kRad TID (Si)
mean that the raditation tests have been performed in order to the value given.
Our customer was looking for an ARM based ready-to-use module (SOM) (which are are quite popular for industrial application) to be used for space application.
could it make sense to come up with a space rated sitara device and work with a partner to have a ready-to-use SOM (with power, RAM, FLASH) that would be space rated?
Rob, Wade, Thanks again for all the comments you provided.
Anthony