How do I Set the timing for the CS signal WRT SCLK? The recommended operating conditions suggests that the delay from the 16th falling edge of SCLK to the rising edge of CS should be a minimum of 0.5 SCLKs, which means (I think) that I should wait until after the rising edge of SCLK before I bring CS high, but the description of CS on page 2 suggests that CS should go high while CLK is low. Can someone help me clear up this confusion?