What is the absolute minimum input voltage on this device such that internal circuits (error amplifier) function properly?
If my input is 1.9V and my desired output is 1.5V with a load current of 300mA then should everything operate correctly? Figure 1 in the datasheet suggests that even with a 500mA output current at 125degC the dropout would be <200mV. Therefore I would still have 200mV headroom. Is that correct?