Other Parts Discussed in Thread: TLV3011
Hello,
We're using the TLV3011-EP comparator to track a nominal 28Vdc input to detect an Undervoltage condition. To reduce power draw and the effect of high-voltage transients, the R1/R2 divider is set at 100k/12.1k. There's also a hysteresis using a 604k resistor. Since this tracking is supposed to be highly accurate over temperature, I'm trying to factor in all the parameters that could affect it and come up with worst-case errors. One of the parameters that comes into play here is the 'Ir' of the ESD or Input pin clamping diodes about which no information is provided in the datasheet. Could you please share the Ir v/s Vr graphs at different temperatures for the internal clamping diodes of this comparator - the nominal and worst-case graphs would be helpful.
Thanks,
Pervaze Humayun.