Part Number: TLV3011-EP
Other Parts Discussed in Thread: TLV3011
Hello,
Looking at the TLV3011 (non-EP) datasheet, the Voltage Reference is specified as [1.230V, 1.242V, 1.254V], which corresponds to 1% accuracy (also specified in the datasheet), hence the [Min, Typ, Max] values corroborate with the specified initial accuracy percentage. This is, however, not the case with TLV3011-EP - 1% accuracy contradicts with [1.208V, 1.242V, 1.276V]. Please clarify which is correct.
Thanks,
Pervaze.