This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848-EP: Compliance of the PHY rise/fall timings vs ANSI X3_263 1995

Part Number: DP83848-EP

Hello,

We are using the DP 83848-EP PHYin an aerospaoce design.

By performing our worst case analysis, we realized that the 100BASE-TX Transmit timings (T2.8.1, min 2.6 ns max 5.5 ns) are not in line with the standard ANSI X3 263 1995 §9.1.6 Rise/fall time., which specifies min 3 ns and max 5 ns.

Is it a reason for this ?

Thank you in advance

Best regards,

PGC

unlocked 2/26/18[LE]