Part Number: TPS7H1101A-SP
Other Parts Discussed in Thread: TPS7H1101-SP
Hi,
The datasheet recommends using Tantalum capacitor (10uF-220uF) with the ESR range of 10 mΩ to 2 Ω along with 0.1uF ceramic capacitor.
please advise on the following:
1. Is there a recommendation regarding the capacitance with respect to the load current? For a low load current (0.2A for example) what input/output capacitance is recommended?
2. For a large load current, I intend to use a 220uF tantalum capacitor. However, the one that I have available has an ESR of 6mOhm. Should I add a 20-30mOhm resistor in series with the capacitor?
3. For a small load current, (0.2A or 0.8A), in case I can use a smaller capacitor, is it OK to use ceramic capacitors (2-3X22uF) with a 20-30mOhm series resistor (in order to comply with the ESR needed for stability)?
Best regards,
Itai