Other Parts Discussed in Thread: MSP430F6459, MSP430WARE
Tool/software: Code Composer Studio
Hi,
we're using MSP430f6459 for one of the application. for the application we've to monitor the frequency signals coming from the external sensors. the sensor data we're processing with some external circuits and given to the Controller. In one test condition we've to test the health of the external circuit. for this we've to feed the internally generated frequency signal to the external circuits using a frequency switcher.
In that case we've to generate 7kHz & 40Hz PWM Signals and capture the same PWM signal to Capture pins of the same timer.
My question : Is it possible to generate PWM signal and capturing the frequency in Same Timer. If possible kindly let us know the suggestions & some examples.
Thank you,
With regards,
Venkata Ramana