Other Parts Discussed in Thread: AM26LV31E, SN65LBC174A-EP, SN65HVD30-EP, SN65HVD10-EP, SN65HVD12-EP, SN55HVD75-EP, AM26LV31
Hi,
I implement RS-422 interface using AM26LV31E-EP, and I am worried about the lightning protection design of the AM26LV31E-EP.
I tried to design each TVS(military of hi-rel grade) on the HI / LO line of AM26LV31E-EP.
Referring to the data sheet of the chip, Maximum input voltage of AM26LV31E-EP is 6V.
But, Most TVS have a clamping voltage above 10V.(Stand off voltage: minimum 5V, Stand off voltage: minimum: 9V)
So, i think that most TVS will not be able to protect the AM26LV31E-EP.
(I think if the 9.2V is injection to the HI / LO pin of AM26LV31E-EP, AM26LV31E-EP will be damaged.)
Am I thinking wrong?
Is there a solution to the lightning protection on the AM26LV31E?
please reply my question.
thanks.