This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS767D301-EP: Reset Output

Part Number: TPS767D301-EP

Hi,

I had followed eZdspTM F28335 design for powering up TMS320F28335SPTPQ in my product. It is the first time power up of my board.

As per the IC functionality, reset time out is 200ms. In my design initial power up sequence is fine. But after that, reset is not stable. It has to be at 3.3V constantly but it is toggling at a period of 4.5 ms.

Signals is like 4.5ms at 3.3V level and 15uS at 0V level and again goes to 4.5mS at 3.3V level. 

Please help me to resolve the issue.