Other Parts Discussed in Thread: UC2832-EP, UC3834, UC2834
Hi I need to get the alternative part for the UC1834. Its a positive/negative regulator. Since UC1834 is costly I need to get a alternative part to test it. Can u suggest one?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi brother,
Input voltage- 5-35V
Output voltage-2.5V-20V
Output current-without pass element (350mA- Driver current), With pass element(8A)
This is military application. I am looking for part which has same architecture of UC1834.
Thanks,
Tharanath