Hi Wade,
I am using SM470R1B1M-HT and have an issue with power on reset of the microcontroller, hopefully can get supports from you.
To have a reliable power on reset, a voltage supervisor (TI TLV803S with 2.93V threshold and 200ms delay) is used to monitor VCCIO which is from a 3.3V DC power supply with a current limit setting of 500mA. VCC (1.8V) is generated by a LDO regulator from the VCCIO and the VCC comes with 5ms delay compared to the VCCIO.
The RESET output of the voltage supervisor is connected to PORRST pin with a 10k pull-up resistor. During the power on reset test, I found that sometimes the microcontroller cannot have a good reset and sank high current from the DC power supply.
I also did another test that the PORRST was connected to GND during power on and then released. I still found that sometimes the microcontroller didn’t stay in reset status when PORRST was held to GND and sank high current from the DC power supply.
Do you have any comments on this case?
Thanks,
Jin