This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS3137-EP: Main crystal value

Part Number: TMS570LS3137-EP

Hi,

For the above device, what is the recommended main crystal value (OSCIN)? I understand that it has to be between 5MHz and 20MHz. 

Many thanks,

Shiromini

  • Shiromini,
    Yes you are correct. 5Mhz to 20Mhz is the input range.
    Selection of actual value used is up to the user, and may depend on other system parameters and performance desired.
    If this answers your question, please click "Verify it as the answer"
    Regards,
    Wade