Hi,
We are using -55 to 175 Deg C part and the input offset voltage should be within +-5mV. Though we are getting almost 9-11mV offset voltage from this part.
Can you please comment on this?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We are using -55 to 175 Deg C part and the input offset voltage should be within +-5mV. Though we are getting almost 9-11mV offset voltage from this part.
Can you please comment on this?
Hello Naman
The Vos limit of +/-5 mV is based on the test conditions shown in the datasheet and are for up to 125C. Above 125C, the limit is +/-11.5C.
If your application is outside these conditions, your results could be different. Also, when measuring Vos, errors in the measurement system and application mismatch must be taken into consideration.
Kirby