This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bootargs parameters to boot with initramfs built in linux kernel



What are the right bootargs parameters which uboot pass to linux for booting with built

in initramfs?

My layout:

omap3evm mistral board(it's not exactly mistral, but very close to), rev G, kernel ver. 2.6.37.

Initramfs image is built from "Arago"  file system, and i can boot using NFS.

I built the image inside the kernel and can't boot using parameters:

mem=220M ip=dhcp console=ttyO2,115200n8

On http://processors.wiki.ti.com/index.php/Initrd page is mentioned that no need in "root=" ,
 "initrd=" need because the fs is built in, but after starting kernel, during boot, on filesystem
 searching I receive an error:
"Unable to mount root fs on unknown-block(2,0)" I don't remember exactly the line, but that's
 the meaning

And another question connected to previous:
 will I have shell(sh) after boot, or i have to run some routines/scripts, without user intervention,
 which will find the real
 File system?

Any help will be appreciated