Other Parts Discussed in Thread: SN74AXC2T45
Hi,
I actually have several questions about the TXS0206 and TXS0206-029. I am new to SD interfaces and after checking the support threads I didn't really find what I was looking for.
- In both devices, how is direction control handled?
- Does the device snoop on the traffic protocol and change direction automatically?
- What is the difference between the TXS0206 Vccb and the TXS0206-029 Vccb O/P?
- They are both fed VccB, so what is the O/P representing?
- Does this just mean Output?
- They are both fed VccB, so what is the O/P representing?
- It appears that TXS0206 WP and CD as well as TXS0206-029 WP/CD pins in the Figure 1 SD Card reference designs are connected to both the Vcca and Vccb power domains.
- What is going on here vs what should go on here?
- Should WP and CD be at Vcca or Vccb?
- If they should be at Vcca then are the TXS0206 and TXS0206-029 WP, CD, and WP/CD pins operating in the Vcca power domain?
- The TXS0206-029 indicates in the terminal functions table on page 3 that WP/CD is only connected to the WP pin at the SD card connector.
- But, the reference design in Fig. 1 on page 2 shows that WP/CD is also connected is to the CD pin at the SD card connector.
- Which is correct, the reference design or the table?
- But, the reference design in Fig. 1 on page 2 shows that WP/CD is also connected is to the CD pin at the SD card connector.
- For the TXS0206-029 how does the WP/CD shared pin function?
- They are separate pins in the TXS0206 and some other devices I've seen.
- Just to be clear, the TXS0206-029 LDO is fixed at 2.9V so this would not be suitable for an SD card requiring 1.8V - correct?
- Will the TXS0206 support SD UHS-I Speed Class 10?
- Would you suggest a different device/family to support SD UHS-I Speed Class 10?
Thank you!