This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G14: VCC=5V interpolation of Vout

Part Number: SN74LVC1G14

Hi Team,

My customer had the following question:

In our circuit, the IC is supplied with 5V and the output of the IC is loaded with 2.6 mA. The output voltage of 3.8 V at VCC 4.5V would not be enough in the circuit, but I am convinced that the IC can deliver a sufficiently high output voltage under the conditions.
Can you tell me how to interpolate the output voltage for this IC so that you can determine the minimum output voltage for VCC 5V?

Thanks in advance and best regards

David