Part Number: SN74AHC1G04-Q1
Hi team
I would like to ask a question related to its spec that:

Vcc is a 3V power supply. Could Vih and Vil can be understood as the input voltage is adjusted from high(such as 12V) to low(such as 0V) or from low to high, Vih is start being controlled by 2.1V, and Vil is start being controlled by 0.9V.
Can it be understood as a Schmidt input converter?