This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LS161A: CLK Input Signal Rise-Time Question

Part Number: SN74LS161A


1) Is V_IH and V_IL from the EC Table in the Datasheet also valid for the CLK Input?
i.e. would the CLK need a voltage higher than 2V(min) to register a rising edge?

2) What is the required rise/fall time of the CLK signal, to make sure a slow transition from Low -> High doesn't cause some kind of glitch?
Would a 1[ns] rise-time though the transition region cause any issues?

3) Assuming the following:
Fclk = 8MHz
LOW = 0V
HIGH = 5V
Duty = 50%

Do you see any issues with a 1[ns] rise-time through the transition region?

Regards,
Darren