A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi ,
i m getting a 2 V pulse in the CLR pin of the 54act74(LCC package) D dflip flop, D and PRE pin is tied to VCC and clock is connectyed to a 10kHz pulse, the CLR pin
is open. the frequency of pulse at the CLR pin is same as the clock frequency.
the same circuit i tested with a 74 act 74 (dip14) the CLR pin voltage was ZERO.
is thee any problem with this IC please help me?????????/
Its likely that the CLR pin is getting pulled up in some way by other circuitry in the system. Whenever there are inputs to a Logic device, it should always be in a defined state and not left floating. Please connect the CLR pin to a pull up or pull down to ensure its input state.
Please note that we are trying to ensure that all posts are answered. With any new posts, we will be sure answer in a timely manner so that no posts go without a response. We will be closing this thread due to its age. Please feel free to post a new thread if you have additional questions, and we would be very happy to help.