Other Parts Discussed in Thread: SN74LVC2G17, SN74LVC1G125
Hi Team
As shown in the figure below, the customer wants to convert one signal into two. Currently, he wants to use the SN74LVC2G07 or do you have any other IC suggestions?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team
As shown in the figure below, the customer wants to convert one signal into two. Currently, he wants to use the SN74LVC2G07 or do you have any other IC suggestions?
The SN74LVC2G07 has open-drain outputs. To get push/pull signals, use the SN74LVC2G17/34.
It might be possible that a signle buffer (SN74LVC1G125) has enough drive strength for two receivers.
The main problem is that the reference design provided by the customer is as follows,
There are two QSPI Flash, the data name is SFIO0~SFIO7 and CS is shared.
At present, I want to divide CS into two CS1 and CS2, but I want to control CS1 or CS2 ON/OFF individually.
If you have other ICs that can be used in this case , please provide me ,THX
That schematic does not show what is connected at the other end of the line.
Anyway, this application does not appear to use open-drain signals. The SN74LVC2G17 or 34 is the correct choice.