This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD4504B-EP: Can CD4504B-EP convert 15Vin to 5Vout?

Part Number: CD4504B-EP


Hi Team, 

My customer is considering CD4504B-EP and he has following questions, could you kindly help? 

1. Can CD4504B-EP convert 15Vin to 5Vout?

2. Is following connection correct to convert 5Vin to 15Vout(High : 15V, Low : 0V)?

VCC = 5V

VDD = 15V

IN = 5V digital signal

OUT = 15V digital signal

VSS = GND

3. Is following connection correct to convert 15Vin to 5Vout(High : 5V, Low : 0V)?

VCC = 15V

VDD = 5V

IN = 15V digital signal

OUT = 5V digital signal 

VSS = GND

4. Can CD4504B-EP convert digital 3.3Vin to 3.3Vout?

5. Is there anything customer should care about when using CD4504B-EP, such as connection or usage? Please let me know if there's any material talking about it. There is no much information in datasheet. 

Thanks.

Regards,

Jo