Other Parts Discussed in Thread: SN74AVC2T45
Hi Team,
I am looking for an AEC-Q part with low tpd.
The application is to make two copies of the same signal (They don't have to be zero delay outputs). tpd is more critical. Lower the better. It is a 1.8V operation.The frequency will be in max of 10Mps or lower.
I did find SN74AVC2T45-Q1 part. For this part, the tpd seem to be 2.5nS @ 1.8V and will be using with Direction control fixed at all the time.
Do we have anything better than this?
This level translator seems to be a bidirectional one. Do you have any concern about using this for uni-directional data passage with respect to reflections and such?
Thank you,
Delaney