Part Number: LSF0204
Hi,
I have any questions.
No. 1: Why is there no pull-up resistance in the A4 and B3 and B4 lines in the data sheet schematics?
Also, please tell me the difference between when pull-up resistance is needed and when it is not.
No. 2: For the A3-B3 line, if A3 is input at 1.8 V, what V is the output signal of B3's High?

Best Regards,
Nishie