This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HCS05: Questions of Input capacitance / Power dissipation capacitance

Part Number: SN74HCS05
Other Parts Discussed in Thread: SN74LV05A

Hi,

My customer has two questions.   Could you please support us?

  • Could you please let us know the typical value of Input capacitance on SN74HCS05PWR?
  • According to the HCS05 datasheet, we can find the Cpd typ.[10pF] under no load test condition.  However, SN74LV05A datasheet said Cpd on both VCC=3.3V case and VCC=5V case under "CL=50pF, F=10MHz test condition".   Can TI provide Cpd of HCS05 under LV05A test condition?  Please advise us.

Thanks and best regards,
M.HATTORI.