This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
We are using SN74LVC1G11DRYR in our design. Kindly suggest a equivalent alternate part for this.
Hi Premalatha,
There are a couple of other package options from the 1G11 if those are options for you (ie if you are already doing a board spin).The 1G11 (3 input AND) is not used as commonly as other options like the SN74LVC2G08 or SN74AUP2G08 (dual 2-input AND). If your design can handle the extra 2 pins of space, these two will have more alternates available and the same function can easily be implemented by connecting 1Y to 2B (adjacent pins) and then your 3 inputs would be 1A, 1B, and 2A, with your output as 2Y.
If you just need to find supply of the SN74LVC1G11 in the DRY package for an existing design, then I would recommend reaching out to your local TI sales office to work with them on lead times for your project / volume / timeline.