This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC07A-Q1: IOL at Vcc=1.8V

Part Number: SN74LVC07A-Q1

Hi,

We can find IOL at VCC=1.65V, 2.3V, 2.7V and 3V in the datasheet as shown in below. 
What is the Low-level output current, IOL at Vcc=1.8V?  

What is the drain voltage when IOL is measured?

Best Regards, Taki