This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AVC4T245: 1.2V to 1.2V straight pass

Part Number: SN74AVC4T245

Hi Expert,

my customer is using SN74AVC4T245 as level shifter 1.2V to1.8V and 1.2V to 3.3V on board. there is an emerging needed, they also want to use 4T245 to cover 1.2V to 1.2V transparent pass scenario.

based on datasheet, I didn't see description for no translation use case. I think Vref 1 and Vref 2 are separated, A port and B port are tracking Vref1 and 2 respectively. both 1.2V could support. could you help to give some advice? Thanks. 

BR

Chi