Part Number: TXS0102
Dear Jimmy
Could you help to check if this chip can run as 6Mhz on SMI bus?(MDC and MDIO)
If not, if there has a P2P solution to support it?
MPN: TXS0102
Bus: SMI bus

Many Thanks,
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Both the MDC and MDIO signals should be push/pull. In this case, the TXS supports up to 22 Mbps.
(The external MDIO pull-up is not needed; the TXS has internal pull-ups.)