This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G240: High-Z of Y when VCC falling (A and /OE low)

Part Number: SN74LVC1G240

Hi,

We have a specific scenario that we would like to ask about with regards to the expected SN74LVC1G240 behavior.

The output (Y) is connected to the gate of an nFET with 1 mega ohm pull-down and 10 uF (actual) capacitance. 
Initial state: VCC = 3V, A high (VCC + 0.5V), /OE connected to A (so high), Y low.

Event #1: A goes low (0V). /OE follows A. Y will try to go high.

Question 1: Will SN74LVC1G240 struggle to charge the 10 uF or potentially be harmed by rush-in current?

Event #2: Event 1 has occured, so A and /OE are low (0V) and Y has managed to go high (VCC). Now VCC is pulled to ground, in practise ending up at ~0.6V.

Question 2: The SN74LVC1G240 will no longer drive the output high, but could we expect Y to go high-Z so that there is no backwards leakage (the only leakage being related to the 1 mega ohm resistor and whatever the capacitor and nFET would bring)?

  • Hi Mr. Engineer,

    1. We spec switching characteristics up to 50pF for this device. 10uF is at risk for exceeding the current maximums of the device. At the minimum you need to add a damping resistor to reduce the current.
    2. Y should be high-Z here.

    Best,

    Malcolm