Other Parts Discussed in Thread: TM4C1294NCPDT
Hi.,
I'm working on TM4C1294NCPDT microcontroller.I transmit the data from one PCB to another PCB.And also receoves the data using CAN communication protocol.
My question is, i transfer the data from CAN in engaged this CAN frame in 8 bytes. I ned to add more frames.For ex:
CAN Initialization:
void CAN1_Initialize(void)
{
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
GPIOPinConfigure(GPIO_PB0_CAN1RX);
GPIOPinConfigure(GPIO_PB1_CAN1TX);
GPIOPinTypeCAN(GPIO_PORTB_BASE, GPIO_PIN_0 | GPIO_PIN_1);
SysCtlPeripheralEnable(SYSCTL_PERIPH_CAN1);
CANInit(CAN1_BASE);
CANRetrySet(CAN1_BASE, true);
CANBitRateSet(CAN1_BASE, g_ui32SysClkFreq, 500000);
CANIntRegister(CAN1_BASE, CAN1IntHandler);
CANIntEnable(CAN1_BASE, CAN_INT_MASTER | CAN_INT_ERROR | CAN_INT_STATUS);
IntEnable(INT_CAN1);
CANEnable(CAN1_BASE);
g_CAN1MsgRx.ui32MsgID = CAN1RXID;
g_CAN1MsgRx.ui32MsgIDMask = 0;
g_CAN1MsgRx.ui32Flags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER;
g_CAN1MsgRx.ui32MsgLen = sizeof(g_ui8CAN1RxData);
CANMessageSet(CAN1_BASE, CAN1RXOBJECT, &g_CAN1MsgRx, MSG_OBJ_TYPE_RX);
CAN Transmission:
void CAN1_Tx_FUNCTION(void)
{
if((g_CAN1MsgRx.ui32MsgID >= 51)&&(g_CAN1MsgRx.ui32MsgID <= 60))
{
uint8_t ui8Count=0;
uint8_t *CAN1_Tx_msgDataPtr;
CAN1_Tx_msgDataPtr = (uint8_t *)&g_ui8CAN1TxData;
for(ui8Count=0 ; ui8Count<sizeof(g_ui8CAN1TxData) ; ui8Count++)
{
g_ui8CAN1TxData[0] =Configuration_No;
g_ui8CAN1TxData[1] = Request_Reply;
g_ui8CAN1TxData[2] = Status;
g_ui8CAN1TxData[3] = RetryAttempt_Count;
g_ui8CAN1TxData[4] =Clearer_Yarn_Status;
g_ui8CAN1TxData[5] =Clearer_Status_Ready;
g_ui8CAN1TxData[6] = Fault_Event;
g_ui8CAN1TxData[7] =Fault_Length;
I have to add more data to transmit another PCB. How to add another CAN frame please guide me or susggest me for any example for adding CAN frame.
If i have to continue g_ui8CAN1TxData[8] =Reserved; or add new frame,how to add.Please give me the solution
Thanks in advance.