This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LSF0108: Voltage on low side too high

Part Number: LSF0108

Hi, I am working on a design with a 5V microcontroller that needs to interface to a 3.3V memory. For this I added a bunch of LSF0108s. For testing purposes I have nothing connected to the low end (A), with the microcontroller I can use GPIO to set each B-side input. When the GPIO is low, the A-side is low too, so far so good. But when the GPIO becomes high (5V) the A-side becomes around 4V. Again, this is with no load connected. The memory chip I'm using specifies its input current as 1uA maximum, so no pull-ups should be necessary I guess. To simulate that load I added a 1.5M resistor from the A-side connection to ground. Then the voltage drops to 3.5 to up to 3.8V. I am afraid to solder the memory chip on the PCB as the higher voltages might damage the device. So why is the voltage on the A-side so high and not clamped to it's 3.3V ref?

This is the schematic: The memory IC is CY14B104