This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Parameters of I2C bus capacitive load

Part Number: PCF8575
Other Parts Discussed in Thread: PCA9548A

Hi,

I use PCF8575 to create new IO lines for microprocessor. I want to calculate total bus capacitance on the I2C bus in order to choose right pull up resistors. So I want to learn that capacitance of P ports (Cio) are adding to total bus capacitance or not. For example Cio of SDA is 7 pF and I use 2 ports which have 10pF each of them. At the end the total bus capacitance of the SDA line between PCF8575 and microprocessor is 27pF?

Also the datasheet said that Cb is the total bus capacitance of one bus line in pF and it is 400pF. So can I understand that SCL and SDA line has 400pF capacitive load separately.

Thanks in advance.