Tool/software:
Hi all,
The datasheet for SN74LVC1G08-Q1 mentions "It can produce 24 mA of drive current at 3.3 V".
It also mentions a 50 mA maximum rating for IO.
I assume that the drive capability is a result of desired output voltage level, i.e. drive current is not internally limited by design.
And I also assume I do need to add external protection if I want to maintain IO < 50 mA.
Is this correct?
Kind regards,
Joey