Tool/software:
Hi, Can you please help me find the maximum power dissipation for this IC
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi, Can you please help me find the maximum power dissipation for this IC
For the actual power consumption, see [FAQ] How do I Calculate Power Consumption or Current Consumption for my CMOS Logic Device?
For the maximum, you have to ensure that the junction temperature does not exceed the TJ limit. So with the DCK package at the maximum ambient temperature, this would be (150 °C − 125 °C) / 293.4 °C/W = 85 mW. (When using the rated output current of 8 mA, the worst-case dissipation is 4.4 mW.)