This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPLD1202: GPIO state during programming via SPI

Part Number: TPLD1202


Tool/software:

Hello Team,

i have a question about the state of GPIO pins during programming.
According to the datasheet the GPIOs are in high impedance mode during startup, until the power on reset is triggered.
In an unprogrammed device the pins should remain in high impedance mode, if I understand that correctly.

Can I be sure that all GPIOs (except the ones that I use for SPI) are staying in the high impedance configuration during the programming via SPI?
I wasn't sure because the datasheet implies that the programming is happening after the POR.


Thank you very much!

Best regards
Renko