Other Parts Discussed in Thread: TVP5158, , TXV0108, TXV0106
Tool/software:
I am using the SN74AVC16T245 to translate +3.3V output of the TI TVP5158 Video Decoder to +1.8V to match an FPGA I/O. The 10 bit data is being clocked out of the TI TVP5158 at 108 MHz.
1. What is the channel to channel skew ?
2. Is the channel to channel skew the same between the two groups of 8 ? For example is the skew for 1B1 to 1A1 the same as 2B1 to 2A1 ??
3. The datasheet states that the max data rates for 1.8V to 3.3V translation is 380 Mbs. Is that for an individual channel ?