This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0106: VCCA slightly greater than VCCB

Part Number: TXB0106

Tool/software:

Hello,

I have VCCA and VCCB powered at 1.8V from two different voltage regulator, so it is possible that VCCA is a little bit greater than VCCB.

For example considering VCCA greater than VCCB by 100mV (VCCA =1.85V and VCCB=1.75V is tollerable or there is some problems with that?

Thank you