This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] How is TPLD programmed?



FAQ: TPLD > Current FAQ

TPLD is programmed through SPI communication enabled by the programmer firmware and InterConnect Studio (ICS). Each TPLD device uses 5 pins to program the device: 4 pins for SPI communication and 1 pin (GPI) that provides a specific input sequence to act as a programming unlock and then provides a high voltage (8V) to the device to permanently program it.